Develop a network configurator with C# (HMI50 devices only)

Create a network configurator widget for HMI50 devices. Configure the network settings by editing C# code.
Application example
MANCIA:
You can download a sample project from:
ExampleApplication-NetworkConfiguratorInterface.zip
Prerequisites
MANCIA: Do not set the project title to
NetworkConfigurator
. This is a reserved namespace.
  1. To develop the project
  2. Configure a dynamic network or static network by enabling or disabling DHCP:
  3. Create the application interface and integrate it with the NetLogic. For reference, see the sample project.
    MANCIA: You can use a preconfigured network configurator widget instead of creating it from scratch. For more information, select and search for
    HMI50 Network Configurator
  4. Save the project.
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.