Add Work Units

Add Work Units

After adding the Work center or Area, you can add the Work units.
NOTE:
The following points are required to view data on
Work units level dashboard
:
  • Data from different meters which are directly connected to a Work Units node will be considered for the data aggregation.
  • For consumption and demand charts, the respective resource meter has to be configured with the proper tag mapping.
  • For Cost charts, the respective rate schedule should be configured at the Site level.
  • For Emission, the respective emission factor should be configured at the Site level.
  • For Production and energy intensity charts should have correct tag mapping for production count measurement.
  • Harmonized units are defined at the Enterprise level and will be used to display harmonized consumption, intensity, or emissions data.
Perform the following steps to add Work units:
  1. Select the
    Area
    or
    Work center
    and the [] icon appears.
  2. Click the [] icon and select [Add].
  3. In the
    Add Component
    dialog, select [Work units] under
    Node
    from the left pane and set these parameters:
    • Type
      : Select the Work units type from the drop-down list.
      Work units types
    • Name
      : Provide the Work units name.
    • Description
      : Provide the description of the Work units.
  4. Click [Add].
The "
Work units added under Work center successfully
" message displays.
Related Information
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.