Add Component
Perform the following steps to add a Component to the Hierarchy list:
- On the left navigation menu, drop-down theConfigurationmenu and clickAsset Setup.
- Click theAssetnode from the Hierarchy list.
- Click the [
] icon and select
Add Node. - In theAdd Nodewindow, set these parameters:
- Name: Provide the Component name.
- Description: Provide a description of the Component.
- Functional Location: Provide the location details.NOTE: Select theAuto Generate Functional Locationcheckbox to use the system-generated functional location.
- Configuration Status: By default, Configuration Status is in Draft, and the user can select the required status from the drop-down list.
- UnderComponent Class Detailssection, set these parameters:
- Component Class Name: Select the required Component Class Name from the drop-down list.
- Component Class Type: Select the required Component Class Type from the drop-down list.
- Operational Regimes: Select the required Operational Regimes from the drop-down list.
- Initial Health Score: Provide an Initial Health Score value in %.
- Commissioned Date: Select the Commissioned date using a date picker.
- ClickAdd.Add ComponentThe "Component was added to hierarchy successfully" message is displayed.
- (Optional) In theInfotab, clickEditand perform the following actions:
- Geographical Location: Provide the Geographical Location details.
- Contact Details: Provide the Contact Details.
- Remarks: Provide the Remarks details.
- Make: Provide the Component Make details.
- Lifecycle Status: Select the required Lifecycle Status from the drop-down list.
- Files Uploaded: ClickBrowseto upload the files related to the Component.
- ClickSave.
To configure
KPI
tab, refer to Configure KPI for Asset and Configure KPI for Component. To configure Sensors
tab, refer to Configure SensorsProvide Feedback