NTP Client view

NTP Client view

Use the
NTP Client
view to view NTP status and to add and delete NTP server addresses.
Use the
NTP Client
view to:
  • View whether the NTP is enabled and the clock is synchronized, and the current time.
  • View the NTP server status.
  • Add NTP server addresses.
  • Specify the preferred NTP servers.
  • Delete NTP server addresses.
TIP:
The parameters in this view are available only when the switch is online and NTP is enabled in the switch.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.