- Stratix device properties
Port Status view
Use the
Port Status
view to view the current status of the active ports. This information is helpful when the switch has link problems such as traffic that is not being received on a switch port.
TIP:
The parameters in this view are available while online.
Provide Feedback