Find available activations
How do I open Find Available Activations?
Click
Manage Activations > Find Available Activations
.Use
icon in the left column. To display the explanation, hover the cursor over the
icon. Possible reasons that an activation is not usable are the activation expired or did not reach its start date.
Find Available Activations
to view paths to available activations and to view the directory path to each activation server. If an activation is not usable, it is marked with a red exclamation mark

The
Path to Activations
list includes all local and all network server locations that were selected to provide activations to this computer. The list is based on the activation search path locations added and selected using the Update Activation Search Path
dialog.The
Available Activations
table lists all available activations. The activations can exist on the local computer or on a remote computer running FactoryTalk Activation Manager
.
TIP:
Activations that are not available for use because of a disconnected Ethernet card or dongle may still appear in
Available Activations
.
TIP:
Node-locked activations and local-only activations on a remote or server computer do not appear in the list of available activations on a client computer. To make these activation types available on a client computer, rehost the node-locked or local-only activations on the server computer and either replace them with concurrent versions or download node-locked or local-only activations to the client computer.
Available Activations
does not indicate if a node-locked activation is not available for use because of a disconnected Ethernet card or dongle.
TIP:
Expired Flexera activations on remote computers that are listed in
Path to Activations
do not appear.The listed activations include:
- The products and activations purchased for each product, and the number of activations used for each product.
- The types of available activations.
- The local computer or remote computer running theFactoryTalk Activation Managersoftware.
Provide Feedback