Distributed Mode Installation

Distributed Mode Installation

  1. If the FTA Activation Service, FTA Security provider and DataView are to be installed on different machines, then install these services in the following order:
    • FTA Activation Service: Run the FactoryTalk Analytics DataView Installer and select [FT Activation Service] and [FT Activation Manager] in the Components Selection section. Refer to FT Activation Service.
    • FTA Security Provider: Run the FactoryTalk Analytics DataView Installer and select [FTA Security] in the Components Selection section. Refer to FTA Security.
    • FTA DataView: Run the FactoryTalk Analytics DataView Installer and select [DataView] in the Components Selection section. Refer to DataView.
  2. Start the following services:
    • FactoryTalk Activation Websocket Service
    • FactoryTalk Activation Service
    • FactoryTalk Activation Helper.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal