Creating Project

Creating Project

A project is a container that isolates and secures the project information such that it can be viewed by only those who have access to the project. By design, an admin or owner of the organization must create a project so that the same can be used by members for pushing data to the platform.
When an admin or an owner in FactoryTalk Hub, creates an organization, a project is provisioned in FactoryTalk DataMosaix. After the admin or owner in FactoryTalk Hub creates the organization, for the very first time when the user clicks FactoryTalk DataMosaix tile in FT Hub, or if the admin tries to sign-in to FactoryTalk DataMosaix, the admin is able to see a message prompting that creating a project is necessary to continue.
Creating a project is a one-time activity. You can create only one project per organization.
Creating a project
When an admin in FT Hub creates an organization and logs in to FactoryTalk DataMosaix for the first time, the following message displays.
Create Project
Click [Create] to intiate project creation.
Project creation begins.
Project creation in progress
After project creation is complete the following tabs display in FactoryTalk DataMosaix.
  • Applications
    - Currently, no applications are visible. A member needs to register an application and generate credentials. These credentials must be configured before the running the application for data visualization. For more information on registering applications, refer Add Application.
    Applications tab
  • Extractor Info
    - Currently, no extractors are visible. A member needs to register an extractor and generate credentials. These credentials must be added in the configuration file. For more information on registering an extractor, refer Add Extractor.
    Extractor Info tab
  • Manage Access
    - Manage Access displays all the members and their roles in the project. As per the tasks, members need to be assigned roles. For example, if a member needs to register an application, the member must be assigned the Data Scientist role. For more information on roles and privileges, refer FactoryTalk DataMosaix Member Roles .
    Manage Access tab
On creation of a project, when you click the [Continue to Main Site] icon, you navigate to Cognite Data Fusion (CDF). When you log in to CDF, you can see the project created in DataMosaix is provisioned in CDF. You can continue to perform further operations on the data in FactoryTalk DataMosaix.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal