Add Area
After adding a Site, you need to add an Area.
NOTE:
The following points are required to view data on
Area level dashboard
:- Data from different meters which are a direct child of the Area node will be considered for data aggregation.
- To show the data of all the available charts, the respective resource meter to be configured with the correct tag mapping.
- For Cost charts, the respective rate schedule should be configured at the Site level.
- For Emission, the respective emission factor should be configured at the Site level.
- For Production, energy intensity charts should have correct tag mapping for production count measurement.
- For more than one resource meter harmonized unit defined at the Enterprise level will be used for displaying data for consumption, intensity & emission.
Perform the following steps to add an Area under Site:
- Select theSiteand the [
] icon appears.
- Click the [
] icon and select [Add].
- In theAdd Componentdialog, select [Area] underNodefrom the left pane and set these parameters:
- Name: Provide the Area name.
- Description: Provide a description of the Area.
- Click [Add].
The "
Area added under Site successfully
" message displays.Related Information
Provide Feedback