Add Region
After adding Enterprise, it is necessary to add location by adding Region.
NOTE:
The following points are required to view data on
Region level dashboard
:- For Cost charts, the respective rate schedule should be configured at the Site level.
- For Emission, the respective emission factor should be configured at the Site level.
- For Production, energy intensity charts should have correct tag mapping for production count measurement.
- For more than one resource meter harmonized unit defined at the Enterprise level will be used for displaying data for consumption, intensity & emission.
Perform the following steps to add a Region under Enterprise:
- Select theEnterpriseand the [
] icon appears.
- Click the [
] icon and select [Add].
- In theAdd Componentdialog, select [Region] underNodefrom the left pane and set these parameters:
- Name: Provide your Country or Region name.
- Description: Provide the description of the Region.
- Click [Add].
The "
Region added to hierarchy successfully
" message displays.Related Information
Provide Feedback