Instruction Set
For information about an instruction, click the category. Click the alphabetical listing to find more information on a specific instruction.
Programming languages are designated as follows.
Ladder Diagram Logic
Function Block
Sequential Function Chart
Structured Text
For more information on Structured Text programming syntax, refer to Structured Text Syntax.
The following list contains the supported languages for each instruction in a category:
Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback